AXIS#.PROFINET.SUPPACTUALVALUEDATA

Description

This command can be used to read the cyclic data sent from the drive to the controller in the configured supplemental telegram. Each index reads a 16-bit word in network byte order.

Example

-->AXIS1.PROFINET.SUPPACTUALVALUEDATA

[0] 49191

[1] 0

[2] 112

[3] 57343

[4] 12059

[5] 0

[6] 0

[7] 0

-->AXIS1.PROFINET.SUPPACTUALVALUEDATA 3

57343

Versions

Action Version Notes
Implemented 02-04-06-000  

General Information

Type Read Only
Units

N/A

Range 0 to 65535
Default Value N/A
Data Type Integer
Stored in Non-Volatile Memory No

Variants Supported

PROFINET drives: AKD2G-SPP

Industrial Ethernet Information

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PROFINET.SUPPACTUALVALUEDATA

5224

Unsigned16[8]

Read Only

-